FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P > CC-Link
FAQ
CC-Link
Where can I set the station number and baud rate?
I want to set the baud rate to 10 Mbps.
I want to set the baud rate to 10 Mbps.
- Category :
Answer
Use Pr.542 to set the station number and Pr.543 to set the baud rate.
To set the baud rate to 10 Mbps, set Pr.543 to "4".
To set the baud rate to 10 Mbps, set Pr.543 to "4".
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700