FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700 > Control terminal
FAQ
Control terminal
Are the multiple terminals SD of the inverter all the same?
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
Yes. (Terminal SDs are connected with each other inside of the inverter.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700