FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P > Operation mode setting
FAQ
Operation mode setting
When the forward rotation signal is input from the external source while Pr.79 (Operation mode) is set to "2" (External operation mode), the RUN LED rapidly blinks and the inverter does not operate.
What is the possible cause?
What is the possible cause?
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
Rapid blinking of the RUN LED indicates that the frequency setting command has not been input or the output stop signal has been input.
Since Pr.79 is set to "2", try inputting the multi-speed signal.
Since Pr.79 is set to "2", try inputting the multi-speed signal.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700