FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ > Operation panel for FR-E500
FAQ
Operation panel for FR-E500
Can I use the operation panel for the FR-E500 with the E700, D700, or F700PJ?
What is necessary to do this?
What is necessary to do this?
- Category :
Answer
The operation panel FR-PA02 for the FR-E500 can be used for these models.
You need the FR-E5P (back cover adapter set) and FR-C20□ (connection cable) for the operation panel.
You need the FR-E5P (back cover adapter set) and FR-C20□ (connection cable) for the operation panel.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ