FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700 > Terminal FM
FAQ
Terminal FM
I want to use the ammeter connected to the terminal FM so that the output current monitor 10 A becomes the full scale.
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
Set Pr.56 (Current monitor reference) to "10A".
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700