FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700 > Switching between PU and NET operation modes
FAQ
Switching between PU and NET operation modes
Can I switch between PU and NET operation modes?
- Category :
Answer
Set Pr.340 (Communication startup mode selection) to "10".
The operation mode can be switched between PU and NET by assigning X65 (PU-NET operation switching) to any of the inverter's input terminals, and then short-circuiting and opening X65-SD.
You can also use the "PU/EXT" key on the operation panel to switch the operation mode.
The operation mode can be switched between PU and NET by assigning X65 (PU-NET operation switching) to any of the inverter's input terminals, and then short-circuiting and opening X65-SD.
You can also use the "PU/EXT" key on the operation panel to switch the operation mode.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700