FAQ
![](/usr/file/attachment/q&a.jpg)
![](/usr/file/attachment/q&a_sp.jpg)
FAQAbout Products
![](/usr/file/attachment/img_mv-1_sm.jpg)
- FAQ > Drive Products > Inverters-FREQROL > NET operation mode
FAQ
NET operation mode
How should I set the inverter to start operation in the NET operation mode when it is powered on?
- Category :
Answer
Set Pr.340 (Communication startup mode selection) to "1" or "2".
Also, by setting Pr.79 (Operation mode selection) to "0", "2", or "6", the inverter enters the NET mode when it is powered on.
Also, by setting Pr.79 (Operation mode selection) to "0", "2", or "6", the inverter enters the NET mode when it is powered on.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700