Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21894
  • Release Date : 2018/08/22 16:29
  • Print

CC-Link, analog output card

Can I use the CC-Link card (FR-A7NC E kit) and the analog output card (FR-A7AY E kit) simultaneously?  
Category : 

Answer

You can install only one option card.
If you want to use two types of cards, replace the inverter with the FR-A700 series.
If you can use RS485 communication instead of CC-Link communication, you can connect a single analog output card to the standard PU connector port.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries