FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700 > CC-Link
FAQ
CC-Link
When operating the inverter via CC-Link, is it necessary to input analog and multi-speed signals from an external source?
Or, can I just input numeric data in words?
Or, can I just input numeric data in words?
- Category :
Answer
If you are using CC-Link just to monitor the inverter and using the analog signal and multi-speed setting to set the frequency, you need to input them externally.
If you are using CC-Link to set the frequency, external signals are not necessary.
You can directly write numeric values to the remote register to operate the inverter.
If you are using CC-Link to set the frequency, external signals are not necessary.
You can directly write numeric values to the remote register to operate the inverter.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700