FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700 > CC-Link
FAQ
CC-Link
I am considering to use the CC-Link option for CC-Link communication.
The Instruction Manual instructs to set consecutive numbers for the station numbers. Can I set reserved stations?
The Instruction Manual instructs to set consecutive numbers for the station numbers. Can I set reserved stations?
- Category :
Answer
You can set reserved and invalid stations.
The Instruction Manual instructs to set consecutive numbers because the master regards an empty number as an error.
The Instruction Manual instructs to set consecutive numbers because the master regards an empty number as an error.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700