FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700 > Frequency setting
FAQ
Frequency setting
I set up an external frequency setting potentiometer and the frequency with the potentiometer turned to the maximum position is initially set to 60 Hz. Can I change it to 90 Hz?
- Category :
-
- FAQ > Drive Products > Inverters-FREQROL
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ
Answer
Set Pr.125 (Terminal 2 frequency setting gain frequency) = "90 Hz".
This changes the frequency with the potentiometer turned to the maximum position (at 5 V input) to 90 Hz.
This changes the frequency with the potentiometer turned to the maximum position (at 5 V input) to 90 Hz.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700