FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700 > FR-Configurator
FAQ
FR-Configurator
Can I use the FR Configurator FR-SW3-SETUP-WJ to operate the inverter?
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
The FR Configurator FR-SW3-SETUP-WJ can only allow for test operation.
Since this is a tool to support the system launch and maintenance, it is not designed for actual operation.
Since this is a tool to support the system launch and maintenance, it is not designed for actual operation.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700