FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ > FR-PU04
FAQ
FR-PU04
I want to use the FR-PU04 used with the 500 series with the 700 series.
Can I set parameters that were not used with the 500 series by the FR-PU04?
Can I set parameters that were not used with the 500 series by the FR-PU04?
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
While the FR-PU04 does not display parameter names, it displays parameter numbers and you can set them.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700