FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700 > Using external potentiometer and multi-speed operation together
FAQ
Using external potentiometer and multi-speed operation together
Can I use an external potentiometer and multi-speed operation together?
If I use them together, which frequency setting is enabled?
If I use them together, which frequency setting is enabled?
- Category :
-
- FAQ > Drive Products > Inverters-FREQROL
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ
Answer
You can use an external potentiometer and multi-speed operation together.
When an external potentiometer signal input and multi-speed setting occur simultaneously, multi-speed setting is prioritized.
When an external potentiometer signal input and multi-speed setting occur simultaneously, multi-speed setting is prioritized.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700