FAQ
![](/usr/file/attachment/q&a.jpg)
![](/usr/file/attachment/q&a_sp.jpg)
FAQAbout Products
![](/usr/file/attachment/img_mv-1_sm.jpg)
- FAQ > Drive Products > Inverters-FREQROL > Terminals P1 and P
FAQ
Terminals P1 and P
When using the brake unit FR-BU2, should I remove the jumper between the terminals P1 and P?
Should I set Pr.30 = "0"?
Should I need to set a percent value in Pr.70?
Should I set Pr.30 = "0"?
Should I need to set a percent value in Pr.70?
- Category :
-
- FAQ > Drive Products > Inverters-FREQROL
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ
Answer
Removal of the jumper between the terminals P1 and P is not necessary unless you are using the DC reactor.
Set Pr.30 = "0" when using the brake unit.
Since setting Pr.30 = "0" invalidates the setting of Pr.70, you do not have to set it.
Set Pr.30 = "0" when using the brake unit.
Since setting Pr.30 = "0" invalidates the setting of Pr.70, you do not have to set it.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700