FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > I want to synchronize the Z200 and E500.
FAQ
I want to synchronize the Z200 and E500.
I want to synchronize speed of the E500 for a new conveyor with the speed of the unit currently using the Z200. How can I do this?
- Category :
Answer
If you are using analog voltage commands, connect the voltage inputs to the FR-E500 and FR-Z200 in parallel to equalize inputs to both units and speeds are synchronized.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E500, FR-Z200