Start main contents

Factory Automation

  • Font Size
  • S
  • M
  • L

Questions

  • No : 21938
  • Release Date : 2018/08/22 16:30
  • Print

Acceleration/deceleration time

The manual explains that the acceleration time and deceleration time are set to the same length of time. Can I enable the acceleration (or deceleration) time only?
Category : 

Answer

You cannot set and/or enable the acceleration time and deceleration time individually.
Product Name
Inverter, magnet motor drive
Product Category
Inverter speed controller
Series
SC-A
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?