FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Peripheral device selection
FAQ
Peripheral device selection
When the inverter is upgraded to a larger capacity than the motor capacity, should I select peripheral devices (MCCB, power factor improving reactor, and others) in accordance with the upgraded inverter capacity?
- Category :
Answer
1. Select the circuit breaker and MC in accordance with the inverter type.
2. Select the power factor improving reactor in accordance with the motor output.
2. Select the power factor improving reactor in accordance with the motor output.
- Product Name
- Inverter, magnet motor drive
- Series
- Others