Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21946
  • Release Date : 2018/08/22 16:30
  • Print

Peripheral device selection

When the inverter is upgraded to a larger capacity than the motor capacity, should I select peripheral devices (MCCB, power factor improving reactor, and others) in accordance with the upgraded inverter capacity?
Category : 

Answer

1. Select the circuit breaker and MC in accordance with the inverter type.
2. Select the power factor improving reactor in accordance with the motor output.
Product Name
Inverter, magnet motor drive
Series
Others

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries