Start main contents

Factory Automation

  • Font Size
  • S
  • M
  • L

Questions

  • No : 21963
  • Release Date : 2018/08/22 16:30
  • Print

Speed 2 operation with potentiometer on operation panel

Is speed 2 switching between the potentiometer on the operation panel and multi-speed operation possible?
During operation using the potentiometer, I want the inverter to decelerate before the operation edge and stop at the edge.
Category : 

Answer

Yes. Set parameters as below.

For FR-E500
Set Pr.79 =3, and Pr.146= 0.
Multi-speed is prioritized.

For FR-S500
Set Pr.79 = 3, and Pr.53 = 1.
Multi-speed is prioritized.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-S500, FR-E500
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?