Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21964
  • Release Date : 2018/08/22 16:30
  • Print

AC reactor and line noise filter wiring

I have the following questions about wiring between the AC reactor and line noise filter:
1. Breaker -> AC reactor (FR-BAL) -> line noise filter (FR-BSF01) -> the inverter
2. Breaker -> line noise filter (FR-BSF01) -> AC reactor (FR-BAL) -> the inverter
Which of the above orders is correct?
Category : 

Answer

Basically, either is OK.
Both orders are electrically identical, but "1" is recommended since it is preferable to place the line noise filter close to the inverter.
If the wiring length between the line noise filter and the inverter is long, the radiation noise from the wiring between them cannot be prevented.
Product Name
Inverter, magnet motor drive
Series
Others

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries