Start main contents

Factory Automation

  • Font Size
  • S
  • M
  • L

Questions

  • No : 21965
  • Release Date : 2018/08/22 16:30
  • Print

Calculation of acceleration/deceleration time

How can I calculate the shortest acceleration/deceleration time?
Category : 

Answer

As the inverter, you can basically use the equation below to calculate the acceleration/deceleration time.
Note that you should consider a factor of 120% for the maximum short-time torque over 0 to 720 r/min for the high-speed series (150% over other rotations per minute).

Acceleration time dt = J dw/(TM α-TL) -> t = J×N/9.55 × (TM α-TLmax)
Deceleration time dt = J dw/(TM β + TL) -> t = J×N/9.55 × (TM β + TLmin)

t: Acceleration/deceleration time [S]
J: Load moment of inertia (total GD2) [N/m2]
N: Rotations per minute [r/min]
TM: Motor rated torque [N?m]
α: Acceleration torque coefficient
β: Braking torque coefficient (regenerative braking torque)
TLmax: Maximum load torque [N?m]
TLmin: Minimum load torque [N?m]
Product Name
Inverter, magnet motor drive
Product Category
Drive unit
Series
Magnetic motor drive
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?