FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Changing parameters
FAQ
Changing parameters
Can I switch between the operation panel potentiometer and current input from an external source with the FR-E520 series inverter?
- Category :
Answer
Before you change Pr.7 and Pr.8, you must switch to the PU operation mode. Switch to the PU operation mode and change them.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-F500