FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Reversible operation of agitator
FAQ
Reversible operation of agitator
For example, when switching from 30 Hz forward rotation to 30 Hz reverse rotation, while the control terminal can switch from the forward to the reverse operation instantaneously, can the inverter switch the rotation direction without a trip?
- Category :
Answer
When the inverter's forward and reverse terminals are switched instantaneously, the inverter decelerates and then switches the rotation direction. It can switch direction without a trip. Figure 1
- Product Name
- Inverter, magnet motor drive
- Series
- Others