FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A500 > Power factor improving effect by option
FAQ
Power factor improving effect by option
If I install the power factor improving converter, AC reactor, DC reactor, line noise filter, and radio noise filter together, how is the power factor improved? Is there any problem by installing all of them?
- Category :
-
- FAQ > Drive Products > Inverters-FREQROL
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A500
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F500
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E500
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-V200
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A200
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-S500
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A100
Answer
Installing the high power factor converter brings the power factor improving effect of 99% or higher.
Therefore, when the high power factor converter is used, it is not necessary to install the AC reactor and DC reactor.
Be sure to install the line noise filter and radio noise filter on the input side of the reactor 1 (FR-HCL01: one of the accessories of the high power factor converter).
Therefore, when the high power factor converter is used, it is not necessary to install the AC reactor and DC reactor.
Be sure to install the line noise filter and radio noise filter on the input side of the reactor 1 (FR-HCL01: one of the accessories of the high power factor converter).
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-S500, FR-E500, FR-A100, FR-F500, FR-A200, FR-A500, FR-V200