FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A500 > Inverter's heat generation quantity
FAQ
Inverter's heat generation quantity
How much heat do FR-A520-3.7K and FR-A520-7.5K generate?
- Category :
Answer
The heat generation quantity while the inverter is outputting the rated current is as follows:
1. FR-A520-3.7K: 230 W
2. FR-A520-7.5K: 420W
The heat generation quantity also varies depending on the output current (motor load factor) and inverter duty. This relationship is graphed in the FR-A500/E500 Technical Material 2.7.2.
1. FR-A520-3.7K: 230 W
2. FR-A520-7.5K: 420W
The heat generation quantity also varies depending on the output current (motor load factor) and inverter duty. This relationship is graphed in the FR-A500/E500 Technical Material 2.7.2.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A500