FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E500 > Parameter unit display
FAQ
Parameter unit display
I use the inverter to rotate a roller and want to monitor the rotations per minute of the roller on the parameter unit.
Can I switch the frequency monitor (or any other monitors) to the roller rotations per minute monitor?
Can I switch the frequency monitor (or any other monitors) to the roller rotations per minute monitor?
- Category :
Answer
Setting Pr.37 to the machine speed at 60 Hz switches the frequency monitor to the rotations per minute monitor.
Note that the speed setting must be input in as the machine speed.
Note that the speed setting must be input in as the machine speed.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E500