FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > Switching between forward and reverse rotations
FAQ
Switching between forward and reverse rotations
How does the inverter operate when the STF signal is turned OFF and then the STR signal is turned ON within the deceleration time?
Is it OK to use the inverter in such a way?
Is it OK to use the inverter in such a way?
- Category :
Answer
When you switch the inverter to the reverse rotation while it is rotating in the forward direction, it decelerates to stop over the deceleration time (set with Pr.8), and then starts rotating in the reverse direction. After switching to the reverse rotation, the inverter accelerates to the specified speed over the acceleration time (set with Pr.7).
Therefore, it is OK to input the reverse signal while the inverter is rotating in the forward direction.
Therefore, it is OK to input the reverse signal while the inverter is rotating in the forward direction.
- Product Name
- Inverter, magnet motor drive
- Series
- Others