FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Accessories > Programmable controllers with no battery (MELSEC-F)
FAQ
Programmable controllers with no battery (MELSEC-F)
Which type of programmable controller from MELSEC-F series has no battery installed?
Answer
A battery is used for backing up program memory and latched device data and maintaining clock operation in the event of a power failure.
The FX3S/FX3G/FX3GC series main units do not use a battery.
For the FX3G/FX3GC series main units, an optional battery can be used.
The FX3S/FX3G/FX3GC series main units do not use a battery.
For the FX3G/FX3GC series main units, an optional battery can be used.
- Product Name
- FX1S, FX1N, FX1NC, FX2N, FX2NC, FX3S, FX3G, FX3GC, FX3U, FX3UC
- Product Category
- Main Unit, Accessories, Options
- Series
- MELSEC-F series