Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22268
  • Release Date : 2018/08/30 13:48
  • Print

External power supply for input(MELSEC-F)

Is it possible to use an external power supply for the 24V DC input (sink input) of a programmable controller?
Category : 

Answer

For the MELSEC-F series, only DC power supply type can use an external power supply.
Product Name
FX1S, FX1N, FX1NC, FX2N, FX2NC, FX3S, FX3G, FX3GC, FX3U, FX3UC
Product Category
Main unit
Series
MELSEC-F series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?