Start main contents

Factory Automation

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22271
  • Release Date : 2018/08/30 13:48
  • Print

How to install a battery to FX3G/FX3GC series

I would like to install an optional battery to the FX3G/FX3GC series.
Category : 

Answer

The FX3U-32BL can be installed to the FX3G/FX3GC series.
After installation, select [Battery Mode: Use the battery] on the FX parameter window of GX Developer or GX Works2.

Please refer to the following manual for further details;
FX3G SERIES PROGRAMMABLE CONTROLLERS USER'S MANUAL(Hardware Edition)
9.3.2 Setting the battery mode
FX3GC SERIES PROGRAMMABLE CONTROLLERS USER'S MANUAL(Hardware Edition)
9.3.2 Setting the battery mode
Product Name
FX3G, FX3GC
Product Category
Main Unit, Accessories, Options
Series
FX3G, FX3GC
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?