FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Network/Communication > Communications using the built-in USB port of the FX3 series
FAQ
Communications using the built-in USB port of the FX3 series
Connection is not established when the built-in USB port of the FX3 series(FX3S/FX3G/FX3GC) is connected to a personal computer(engineering tool).
- Category :
-
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series
- FAQ > Controllers > Programmable Controllers MELSEC > Engineering Software
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Main Unit
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Network/Communication
Answer
When you connect the built-in USB port of the FX3 series to the personal computer for the first time, you need to install the USB driver into the personal computer.
The installer is in the USBDriver folder which can be found under the Easysocket folder (in a folder used to install GX Developer or GX Works2).
The installer is in the USBDriver folder which can be found under the Easysocket folder (in a folder used to install GX Developer or GX Works2).
- Product Name
- FX3S, FX3G, FX3GC
- Product Category
- Main Unit, Network/Communications, Engineering Software, GX Developper, GX Works2
- Series
- FX3S, FX3G, FX3GC