Start main contents

Factory Automation

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22284
  • Release Date : 2018/08/30 13:48
  • Update : 2019/02/18 15:17
  • Print

I/O structure error in the MELSEC-F

M8060 (I/O structure error) turns on in the MELSEC-F series and 1020 is stored in D8060.
What does that mean?
Category : 

Answer

When an unimplemented input (X) or output (Y) number is used in a program, M8060 turns on.
The first to third digits of the numerical value stored in D8060 indicate the device number.
The fourth digit indicates the I/O type as input (1) or output (0).
When the numerical value is 1020, the inputs X20 and later used in a program are not implemented.
Product Name
FX1S, FX1N, FX1NC, FX2N, FX2NC, FX3S, FX3G, FX3GC, FX3U, FX3UC
Product Category
Main unit, Engineering Software, GX Developper, GX Works2
Series
MELSEC-F series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?