Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • No : 23596
  • Release Date : 2018/09/14 15:09
  • Print

M-code

Answer

"M-code" is outputted to turn ON/OFF machine's solenoids or relays according to the start/end of the positioning operation.
The following two modes are selectable.
• WITH mode: The M-code ON signal is turned ON at the positioning start
• AFTER mode: The M-code ON signal is turned ON at the positioning completion
Product Name
Simple Motion module/
Positioning module
Series
MELSEC iQ-R
MELSEC iQ-F
MELSEC-Q
MELSEC-L

May I have your opinion?

Inquiries