Start main contents

Factory Automation

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23599
  • Release Date : 2018/09/14 15:09
  • Print

Home position address

Answer

Set "[Pr.45] Home position address (72+150n, 73+150n)" of the basic parameters for home position return.
Set by 2 words.
The value will be reflected when PLC ready signal is turned OFF to ON.

(Note): "n" = number of axes - 1.
Product Name
Simple Motion module/
Positioning module
Series
MELSEC iQ-F
MELSEC-Q
MELSEC-L
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?