FAQ


FAQAbout Products
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Positioning Modules > QD75MH > Home position address
FAQ
Home position address
In order to set the home position address except "0" by data set method home position return, what buffer memory address should I write the data to?
- Category :
-
- FAQ > Controllers > Motion Controllers > MELSEC iQ-F Series > Simple Motion Modules > FX5SSC
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Simple Motion Modules > QD77MS
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Simple Motion Modules > QD77GF
- FAQ > Controllers > Motion Controllers > MELSEC-L Series > Simple Motion Modules > LD77MS
- FAQ > Controllers > Motion Controllers > MELSEC-L Series > Simple Motion Modules > LD77MH
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Positioning Modules > QD75MH
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Positioning Modules > QD75M
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Positioning Modules > QD74MH
Answer
Set "[Pr.45] Home position address (72+150n, 73+150n)" of the basic parameters for home position return.
Set by 2 words.
The value will be reflected when PLC ready signal is turned OFF to ON.
(Note): "n" = number of axes - 1.
Set by 2 words.
The value will be reflected when PLC ready signal is turned OFF to ON.
(Note): "n" = number of axes - 1.
- Product Name
- Simple Motion module/
Positioning module
- Series
- MELSEC iQ-F
MELSEC-Q
MELSEC-L