Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 23614
  • Release Date : 2018/09/14 15:09
  • Print

Error 1205

Answer

Error 1205 (SSCNET communication error) occurs when erroneous data is received from servo amplifier.

[When the servo parameter "[PA14] Rotation direction selection/travel direction selection" is changed]
Execute the home position return again.

[When the servo parameter "[PA14] Rotation direction selection/travel direction selection" is not changed]
• Check if the SSCNETIII cable and the encoder cable are connected correctly.
• Take measures against noise.
Product Name
Simple Motion module/
Positioning module
Series
MELSEC-Q
MELSEC-L

May I have your opinion?

Inquiries