FAQ
FAQAbout Products
- FAQ > Controllers > Motion Controllers > MELSEC-L Series > Simple Motion Modules > LD77MS > Error 2035
FAQ
Error 2035
What is error 2035?
What should I do when it occurs?
What should I do when it occurs?
- Category :
-
- FAQ > Controllers > Motion Controllers > MELSEC iQ-R Series > Simple Motion Modules > QD77MS
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Simple Motion Modules > QD77GF
- FAQ > Controllers > Motion Controllers > MELSEC-L Series > Simple Motion Modules > LD77MS
- FAQ > Controllers > Motion Controllers > MELSEC-L Series > Simple Motion Modules > LD77MH
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Positioning Modules > QD75MH
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Positioning Modules > QD75M
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Positioning Modules > QD74MH
Answer
Error 2035 (Command frequency error) occurs when the servo amplifier detects a command frequency error.
(1) When the command from the controller is the permissible speed or higher.
• Check operation pattern.
(2) When the command is lower than the permissible speed.
• Take countermeasure against I/O signal noise
• Take countermeasure against servo system controller noise
Refer to relevant servo amplifier manuals for details.
(1) When the command from the controller is the permissible speed or higher.
• Check operation pattern.
(2) When the command is lower than the permissible speed.
• Take countermeasure against I/O signal noise
• Take countermeasure against servo system controller noise
Refer to relevant servo amplifier manuals for details.
- Product Name
- Simple Motion module/
Positioning module
- Series
- MELSEC-Q
MELSEC-L