FAQ


FAQAbout Products
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Positioning Modules > QD75MH > HPR request flag
FAQ
HPR request flag
When does the "HPR request flag" turn ON?
- Category :
-
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Simple Motion Modules > QD77MS
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Simple Motion Modules > QD77GF
- FAQ > Controllers > Motion Controllers > MELSEC-L Series > Simple Motion Modules > LD77MS
- FAQ > Controllers > Motion Controllers > MELSEC-L Series > Simple Motion Modules > LD77MH
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Positioning Modules > QD75MH
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Positioning Modules > QD75M
Answer
It depends on the setting of servo parameter "[PA03] Absolute position detection system" whether the HPR request flag ("[Md.31] Status": b3) turns ON or not.
The flag turns ON in the following cases:
(1) "1: Enabled (absolute position detection system)"
• When the machine HPR has not been executed at the absolute position system
• When a machine HPR operation starts
• When the absolute system has not been set
• When "[PA14] Rotation direction selection/travel direction selection" is changed
(2) "0: Disabled (incremental system)"
• System's power supply on or reset
• Servo amplifier power supply on
• Machine HPR start
The flag turns ON in the following cases:
(1) "1: Enabled (absolute position detection system)"
• When the machine HPR has not been executed at the absolute position system
• When a machine HPR operation starts
• When the absolute system has not been set
• When "[PA14] Rotation direction selection/travel direction selection" is changed
(2) "0: Disabled (incremental system)"
• System's power supply on or reset
• Servo amplifier power supply on
• Machine HPR start
- Product Name
- Simple Motion module/
Positioning module
- Series
- MELSEC iQ-R
MELSEC iQ-F