Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 24680
  • Release Date : 2019/02/22 11:39
  • Update : 2019/02/22 14:03
  • Print

1 ms timer (FX3G/3GC series)

Is there a 1 ms timer in the FX3G/3GC series?
Category : 

Answer

Yes, there is.
T256 to T319 can be used for the1 ms timer, and T246 to T249 can be used for the 1 ms retentive timer.
Product Name
FX3G, FX3GC
Product Category
Main unit, Engineering Software, GX Developer, GX Works2
Series
MELSEC-F series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?