Start main contents

Factory Automation

  • Font Size
  • S
  • M
  • L

Questions

  • No : 24681
  • Release Date : 2019/02/22 11:40
  • Update : 2019/02/22 14:15
  • Print

Comment display

Although a comment is read from a programmable controller, it is not displayed on the window of GX Works2.
Category : 

Answer

The comment may not have been written to the programmable controller.
Or, the comment display setting may be required on the GX Works2 side.

[Writing a comment to a programmable controller using GX Works2]
・ Setting a comment capacity
 On the Project view of the Navigation window, select "Parameter" → "PLC Parameter". Click the "Memory Capacity" tab, and set the comment capacity in "Comments Capacity". ("1" block, "50" points)
・ Writing a comment
 Select "Online" → "Write to PCL" from the menu. Select "Global Device Comment", and click the "Execute" button.

[Setting comment display on GX Works2]
 Select "View" → "Comment" from the menu.
Product Name
FX1S, FX1N, FX1NC, FX3S, FX3G, FX3GC, FX2N, FX2NC, FX3U, FX3UC
Product Category
Main unit, Engineering Software, GX Developer, GX Works2
Series
MELSEC-F series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?