FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Main Unit > Comment display
FAQ
Comment display
Although a comment is read from a programmable controller, it is not displayed on the window of GX Works2.
Answer
The comment may not have been written to the programmable controller.
Or, the comment display setting may be required on the GX Works2 side.
[Writing a comment to a programmable controller using GX Works2]
・ Setting a comment capacity
On the Project view of the Navigation window, select "Parameter" → "PLC Parameter". Click the "Memory Capacity" tab, and set the comment capacity in "Comments Capacity". ("1" block, "50" points)
・ Writing a comment
Select "Online" → "Write to PCL" from the menu. Select "Global Device Comment", and click the "Execute" button.
[Setting comment display on GX Works2]
Select "View" → "Comment" from the menu.
Or, the comment display setting may be required on the GX Works2 side.
[Writing a comment to a programmable controller using GX Works2]
・ Setting a comment capacity
On the Project view of the Navigation window, select "Parameter" → "PLC Parameter". Click the "Memory Capacity" tab, and set the comment capacity in "Comments Capacity". ("1" block, "50" points)
・ Writing a comment
Select "Online" → "Write to PCL" from the menu. Select "Global Device Comment", and click the "Execute" button.
[Setting comment display on GX Works2]
Select "View" → "Comment" from the menu.
- Product Name
- FX1S, FX1N, FX1NC, FX3S, FX3G, FX3GC, FX2N, FX2NC, FX3U, FX3UC
- Product Category
- Main unit, Engineering Software, GX Developer, GX Works2
- Series
- MELSEC-F series