Start main contents

Factory Automation

  • Font Size
  • S
  • M
  • L

Questions

  • No : 24687
  • Release Date : 2019/02/22 11:44
  • Update : 2019/02/22 15:22
  • Print

Battery consumption while the programmable controller is powered on

Will the battery voltage become low if a programmable controller is powered on all the time?
Category : 

Answer

A battery is consumed regardless of the on/off state of the programmable controller.
Refer to the User's Manual (Hardware Edition) for the module used, and replace the battery periodically.

For example, the life of the FX3U-32BL battery is approximately 5 years (ambient temperature: 25ºC ).
The battery life varies depending on ambient temperatures. Estimate the battery life according to the graph, and replace the battery periodically.
Product Name
FX1S, FX1N, FX1NC, FX3S, FX3G, FX3GC, FX2N, FX2NC, FX3U, FX3UC
Product Category
Main unit, Options, Accessories
Series
MELSEC-F series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?