Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 24692
  • Release Date : 2019/02/27 08:56
  • Print

Comparison result of the CMP instruction

When the CMP instruction is executed, the comparison result is not cleared even after the command input turns off.
Category : 

Answer

A comparison result is held even after the command input turns off. The remaining comparison result can be cleared by using the RST or ZRST instruction.
Product Name
FX1S, FX1N, FX1NC, FX3S, FX3G, FX3GC, FX2N, FX2NC, FX3U, FX3UC
Product Category
Main unit, Engineering Software, GX Works2, GX Developer
Series
MELSEC-F series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?