FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Main Unit > Latch (backup) areas in the data register (D) and extended register (R) of the FX3U/FX3UC series
FAQ
Latch (backup) areas in the data register (D) and extended register (R) of the FX3U/FX3UC series
Which areas in the data register (D) and extended register (R) of the FX3U/FX3UC series can be latched?
Answer
D200 to D7999 and R0 to R32767 can be latched.
D200 to D511 can be set as non-latch areas in parameters.
For details on the parameter setting, refer to the following.
Section 2.7.9 (3 Setting devices) in the FX3S/FX3G/FX3GC/FX3U/FX3UC Series Programmable Controllers Programming Manual [Basic & Applied Instruction Edition] (Manual number: JY997D16601)
D200 to D511 can be set as non-latch areas in parameters.
For details on the parameter setting, refer to the following.
Section 2.7.9 (3 Setting devices) in the FX3S/FX3G/FX3GC/FX3U/FX3UC Series Programmable Controllers Programming Manual [Basic & Applied Instruction Edition] (Manual number: JY997D16601)
- Product Name
- FX3U, FX3UC
- Product Category
- Main unit, Engineering Software, GX Works2, GX Developer
- Series
- MELSEC-F series