Start main contents

Factory Automation

  • Font Size
  • S
  • M
  • L

Questions

  • No : 24700
  • Release Date : 2019/02/27 08:59
  • Print

Maximum number of characters in a comment that can be transferred to a FX3U series

How many characters in a comment can be transferred to FX3U series?
Category : 

Answer

As project data, up to 32 one-byte characters (16 two-byte characters) can be input to each global device comment. However, the maximum number of characters that can be written to a programmable controller is 16 (one-byte) (8 (two-byte)).
(Local device comments cannot be written to the MELSEC-F series. To write local device comments, create them as global device comments, or convert them to global device comments before writing to the MELSEC-F series.)
Product Name
FX3S, FX3G, FX3GC, FX3U, FX3UC
Product Category
Main unit, Engineering Software, GX Works2, GX Developer
Series
MELSEC-F series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?