Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 24706
  • Release Date : 2019/02/27 09:00
  • Print

FX3U-ENET-ADP connectable programmable controllers in the MELSEC-F series

Are there any FX3U-ENET-ADP (for Ethernet communications) connectable programmable controllers in the MELSEC-F series?
Category : 

Answer

The FX3U-ENET-ADP can be connected to the FX3G/FX3GC series (both Ver. 2.00 or later) and the FX3U/3UC series (both Ver. 3.10 or later).
Products which are required for connecting the FX3U-ENET-ADP to the above programmable controllers can be checked using MELSEC-F Series Model selection tool.

* The version of main units can be checked on the "PLC Diagnostics" window of GX Works2 or by monitoring the last three digits of the data in D8001 (PLC type and system version).
* When connecting to the FX3G series, a connector conversion adapter, FX3G-CNV-ADP, is required.
* When connecting to the FX3U series or the FX3UC-32MT-LT(-2), an expansion board, for example, FX3U-CNV-BD, is required.
Product Name
FX3U-ENET-ADP
Product Category
Main unit, Engineering Software, Network/Communication GX Developer, GX Works2
Series
FX3G, FX3GC, FX3U, FX3UC

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries