Start main contents

Factory Automation

  • Font Size
  • S
  • M
  • L

Questions

  • No : 24768
  • Release Date : 2019/02/27 15:01
  • Print

Externally switching the operating status of a programmable controller

How can I externally switch the operating status of a programmable controller?
Category : 

Answer

On the Project view of the Navigation window, select "Parameter" → "PLC Parameter" using GX Works2 (or GX Developer). Click the "PLC System(1)" tab, and set the "RUN Terminal Input".
Connect a switch to the RUN terminal set in parameter and transfer program/parameters from the personal computer to the programmable controller. Then, the operating status can be changed using the switch connected.
To enable the RUN/STOP operation by using the switch connected, keep the RUN/STOP switch of a programmable controller in the STOP position.
Product Name
FX1S, FX1N, FX1NC, FX3S, FX3G, FX3GC, FX2N, FX2NC, FX3U, FX3UC
Product Category
Main unit, Engineering Software, GX Works2, GX Developer
Series
MELSEC-F series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?