Start main contents

Factory Automation

  • Font Size
  • S
  • M
  • L

Questions

  • No : 24771
  • Release Date : 2019/02/27 15:17
  • Print

External appearance of the F2-40BL

The shapes of the F2-40BL battery differ between the one installed and the one separately available (spare part).
Category : 

Answer

Some of the F2-40BL batteries installed to a programmable controller are mounted on the printed circuit board. The separately available F2-40BL batteries (spare parts) are not mounted on a printed circuit board. The both types have the same function.
Product Name
F2-40BL
Product Category
Accessories, Options
Series
FX2N
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?