Start main contents
Font Size
S
M
L
FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC-F Series
>
Main Unit
>
Scan time while operation of a progra...
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
No : 24779
Release Date : 2019/02/27 15:58
Print
Scan time while operation of a programmable controller CPU is being monitored using GX Works2
While operation of a programmable controller CPU is being monitored using GX Works2, the scan time displayed differs from the expected scan time.
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
Scan time displayed on GX Works2 is the maximum scan time of the monitor target programmable controller CPU.
To check current scan time, monitor the data in D8010.
Product Name
FX1S, FX1N, FX1NC, FX3S, FX3G, FX3GC, FX2N, FX2NC, FX3U, FX3UC
Product Category
Main unit, Engineering Software, GX Works2, GX Developer
Series
MELSEC-F series
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
Data backup failure
Keyword protection of the MELSEC-F se...
COM terminal for outputs
Distinguishing the usage of standard ...
How to check the version of the MELSE...
page top
HOME
FAQ